Technical FAQs

Ask a Question

What type of stainless steel is used for NEMA 4/4X/5 stainless steel circuit breaker enclosures?

Type 304 stainless steel is used. Type 316 stainless steel is not available.


CTA-ID : 9304
Was this helpful?
What can we do to improve the information ?