Technical FAQs

Ask a Question

What are the repair parts for a HU464AWK Series E1 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40560-273-50 (arc suppressor is included)
Arc suppressor assembly - 40512-706-50
Lug Assembly - CL20F (incl. 6 lugs)
Line base phase insulator - 40520-253-01
Cross bar insulator - 40511-390-01
Dust shield - 40511-391-01
Mechanism insulator - 40511-371-01
Line base mounting screws - 40205-065-01
Handle knob kit - 4028344050K ( Series E Switches only)


CTA-ID : 9292
Was this helpful?
What can we do to improve the information ?