Technical FAQs

Ask a Question

For the American market,can we use a VIGI associated to a NS100, i.e. are the Vigi module UL 508 certified?

NO, the VIGI modules are not UL, =S= has not asked for it, based on 2 main reasons :
- the electronic card in the Vigi module is not UL; to change it would require a redesign
So far the sales volume does not justify the cost linked to the technical evolution and UL certification.

CTA-ID : 9720
Was this helpful?
What can we do to improve the information ?