Technical FAQs

Ask a Question

When using maintened signals with a ``TS`` type motor mechanism, do we need to disconnect B4 terminal ?

When using maintained signals with a ``TS`` type motor mechanism, B4 terminal has to be disconnected. (connection of B4 only for the T motor mechanism).


CTA-ID : 9719
Was this helpful?
What can we do to improve the information ?