Technical FAQs

Ask a Question

PDC12MA4 lug: What is the mounting screw torque, conductor size and wire binding screw torque for this distribution lug?

Mounting screw torque: 180 lb-in.
Conductor qty and size: 12 maximum
#6-#4 Cu at 35 lb-in.
#8 AWG Cu at 25 lb-in.
#10 AWG Cu at 20 lb-in.

CTA-ID : 9716
Was this helpful?
What can we do to improve the information ?