Technical FAQs

Ask a Question

PDC6LA20 lug: What is the mounting screw torque, conductor size and wire binding screw torque for this distribution lug?

Mounting screw torque: 180 lb-in.
Conductor qty and size: 6 maximum
#3-#2/0 AWG Cu at 50 lb-in.
#6-#4 AWG Cu at 45 lb-in.
#8 AWG Cu at 40 lb-in.
#12-#10 AWG Cu at 35 lb-in.

CTA-ID : 9713
Was this helpful?
What can we do to improve the information ?