Technical FAQs

Ask a Question

For IEC applications, can a combusbar be used under DC? If yes, what is the maximum operating voltage?

Yes, the combusbar for C60 can be used under DC. The rated insulation voltage = 500 V.

CTA-ID : 9706
Was this helpful?
What can we do to improve the information ?