Technical FAQs

Ask a Question

May the C120 and NG125 be applied at 400 Hz?

DO NOT USE C120 and NG125 under 400 Hz (the magnetic threshold is too high, and the self-protection of the device won`t be guaranteed)


CTA-ID : 9705
Was this helpful?
What can we do to improve the information ?