Technical FAQs

Ask a Question

What is the grade (gauge) of stainless steel used in the manufacturing of both the NEMA 3R stainless steel and NEMA 4 stainless steel enclosures?

The grade of stainless steel used in manufacturing these enclosures is 304.

(Updated 2/27/03)


CTA-ID : 9458
Was this helpful?
What can we do to improve the information ?