Technical FAQs

Ask a Question

What are the repair parts for a H224DS Series E1 Heavy Duty Safety Switch?

Issue:
Previous design Repair parts

Product Line:
Heavy Duty Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The parts listed here are the only field replaceable parts.
Line base assembly - 4056027550 (arc suppressor is included) (Obsolete, NLA with No Replacement)
Load base assembly - 4056027650 (Obsolete, NLA with No Replacement)
Arc suppressor assembly - 4051270650 (Obsolete, NLA with No Replacement)
Lug Assembly - CL20F (incl. 6 lugs)
Cross bar insulator - 4051136101 (Obsolete, NLA with No Replacement)
Dust shield - 4051136201
Mechanism insulator - 4051137101 (Obsolete, NLA with No Relacement)
Line and load base mounting screws - 4020506501
Handle knob kit - 4028344050K ( Series E Switches only)

 
Was this helpful?
What can we do to improve the information ?