Technical FAQs

Ask a Question

What are the repair parts for a H224A Series E1 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40560-275-50 (arc suppressor is included)
Load base assembly - 40560-276-50
Arc suppressor assembly - 40512-706-50
Lug Assembly - CL20F (incl. 6 lugs)
Cross bar insulator - 40511-361-01
Dust shield - 40511-362-01
Mechanism insulator - 40511-371-01
Line and load base mounting screws - 40205-065-01
Handle knob kit - 4028344050K ( Series E Switches only)


CTA-ID : 9276
Was this helpful?
What can we do to improve the information ?