Technical FAQs

Ask a Question

What are the repair parts for a HU464 Series E1 Heavy Duty Safety Switch?

Obsolete design repair parts

Product Line:
Heavy Duty Safety Switches

Repair parts


The parts listed here are the only field replaceable parts.
Line base assembly - 40560-283-50 (OBSOLETE AND NO LONGER AVAILABLE)
Arc suppressor assembly - 40512-706-50 (4 required)
Lug assembly - 40251-162-51 (8 required)
Line base phase insulator - 40520-253-01 (3 required)
Cross bar insulator - 40511-390-01
Dust shield - 40511-391-01
Mechanism insulator - 40511-371-01
Line and load base mounting screws - 40205-065-01 (2 required per base)
Handle knob kit - 4028344050K ( Series E Switches only)

CTA-ID : 9275
Was this helpful?
What can we do to improve the information ?