Technical FAQs

Ask a Question

What are the repair parts for the HU664DS, series F5? (may be shown as F05)

The repair parts for the HU664DS, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056704350 - (requires one base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Complete Line/Load Base mounting screws - 40205-142-02 (requires 12 per base)
Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 21401-222-40 (per lug)
Switch Mechanism - 40567-401-50 (also requires mechanism coupling assembly 40566-998-50 and interlock connector assembly 40567-188-50)
Switch Mechanism mounting screws- 21949-181-21 (requires 2)
Handle Assembly - 40567-368-50
Lockplate - 40567-389-01
Lockplate mounting screws - 21949-181-21 (requires 2)

CTA-ID : 8965
Was this helpful?
What can we do to improve the information ?