Technical FAQs

Ask a Question

Is it possible to use a DPN VIGI under 24VAC/50Hz ?

The MCB and earth leakage function will operate under 24V. But the test circuit won`t operate. The minimum voltage is 104V for the button test.



CTA-ID : 9690
Was this helpful?
What can we do to improve the information ?