Technical FAQs

Ask a Question

Customer wants to know if the HOM120AFI breaker will cause radio interference.

This is not likely when properly applied and installed. The instructions state, however, that this is a possibility due to the properties of the breaker, and further action recommendations are given on the instructions.

CTA-ID : 9689
Was this helpful?
What can we do to improve the information ?