Technical FAQs

Ask a Question

What is the difference between an MHC**(S or F) and MHC**V(S or F)?

The MHC**V(S or F) is a vented trim used on 400 and 600 amp NQOD panels. The MHC**(S or F) is a a non vented trim used on 100 and 225 amp NQOD panels. They are not interchangeable.


CTA-ID : 9453
Was this helpful?
What can we do to improve the information ?