Technical FAQs

Ask a Question

Can three (3) electrical accessories be installed in an FAL circuit breaker? A shunt trip, UVR, and an aux. switch?

Unfortunately, it is not possible to install these three accessories on an FAL circuit breaker. They each require an outside pole for mounting, and there are only two outside poles. Three accessories can be installed only if one of them is an alarm switch (bell-alarm) which goes in the center pole.



CTA-ID : 9451
Was this helpful?
What can we do to improve the information ?