Technical FAQs

Ask a Question

When the customer presses the button on the ammeter on an SE breaker, the battery symbol comes on. Does this mean the battery is bad? Can it be replaced?

No, it means the battery is good. No indication would mean it`s bad. The battery cannot be replaced.


CTA-ID : 9447
Was this helpful?
What can we do to improve the information ?