Technical FAQs

Ask a Question

Wants to order a 35636 CK breaker escutcheon with Kirk key provision), but the system won`t let him.

The Kirk key provision can be done only in the factory. A cover with provision is not available because we do not have spare covers. It can be installed if the breaker is sent back to the factory with a ``Return for Repair`` RMA.


CTA-ID : 9680
Was this helpful?
What can we do to improve the information ?