Technical FAQs

Ask a Question

Testing SED with ground fault. If I do not have a SEPITK2 adapter plug kit, how can I reestablish the secondary connection jumper wires for testing out of the cell?

Jumper terminal 16 to 19. For ground fault breakers.
Jumper terminal 17 to 18. For ground fault breakers.
Jumper terminal 20 to 21. For ground fault breakers.
Jumper terminal 23 to 24. Short time delay self restraint.
To defeat Ground fault during primary injection place an additional jumper from terminal 16 to 17.


CTA-ID : 9677
Was this helpful?
What can we do to improve the information ?