Technical FAQs

Ask a Question

NSF/NSJ door mounted operating handle: What is the degree of protection?

The handle mechanism can be used in NEMA 3R and 12 enclosure applications.
Degree of protection: IP40 as per IEC 529.


CTA-ID : 9439
Was this helpful?
What can we do to improve the information ?