Technical FAQs

Ask a Question

Which AC voltages are available for the NSJ motor operator?

The motor operator for the NSJ is available in the following AC voltages:
Voltage Suffix Scroll down for all options
48/60 ML
110/130 MA
208/277 MD
380/415 MF
440/480 MH

CTA-ID : 6346
Was this helpful?
What can we do to improve the information ?