Technical FAQs

Ask a Question

Can we use LED`s in standard full voltage 9001 KM light modules or in 9001 KM transformer light modules?

You can use 6 volt LED`s in any transformer light module. In full voltage you must use an LED of the correct voltage. We don`t offer LED`s in all these voltages. The 9001 KM LED light modules all have resistors that drop the voltage to 12 volts.


CTA-ID : 8163
Was this helpful?
What can we do to improve the information ?