Technical FAQs

Ask a Question

Why can`t a 9001 KX illuminated operator be ordered with a shallow depth light module?

Due to several locating nibs and slots on the KX mounting collar the shallow depth light module will not mount flush to the mounting collar. This light module was developed to use with the 9001 K and 9001 SK units. It was originally developed so an illuminated push button could be mounted in a 9001 SKYP pendant station.

CTA-ID : 8155
Was this helpful?
What can we do to improve the information ?