Technical FAQs

Ask a Question

Why does Altivar ATV58 with a General Purpose Option card not retain the settings?

The GPO card settings are not immediately saved when a user pressed the enter key.
Upon final programming of the option card users must go to Menu 8 parameter 1, and change the value to 1. This will store the GPO settings in the option card and re-write Parameter 1 to 0.
Failure to do so will result in the GOP card reloading the previously stored configuration (typically factory default) back into the drive at the next power up, run command, audition, or command for DC injection.

CTA-ID : 8152
Was this helpful?
What can we do to improve the information ?