Technical FAQs

Ask a Question

What wire sizes can be used with the M9 IEC 947-2 Rated NC100 Circuit Breaker?

Cable range : pressure terminals are suitable for solid copper cables:
10 to 100A : 35mm^2 stranded or 50mm^2 solid


CTA-ID : 6257
Was this helpful?
What can we do to improve the information ?