Technical FAQs

Ask a Question

What is an RCBO?

An RCCB is a switch (no thermal-magnetic overcurrent protection) with ground-fault protection. By contrast, an RCBO is more like our GFI breaker with thermal-magnetic protection in addition to ground-fault protection. ``Residual`` simply means ground current. They are IEC rated (not UL), so their use is only for OEMs who want these product features and don`t need UL listing on the devices.

CTA-ID : 6218
Was this helpful?
What can we do to improve the information ?