Technical FAQs

Ask a Question

What is the terminal layout for push-in connector installation for the Masterpact NW drawout breaker?

A terminal layout for the drawout breaker is in the instruction bulletin provided with the NW breaker. Document number 48049-106-03 page 23.

CTA-ID : 6199
Was this helpful?
What can we do to improve the information ?