Technical FAQs

Ask a Question

What standards do Masterpact NW/NT breaker comply with?

These breakers comply with the following standards.
Low -Voltage Power Circuit Breaker (Drawout)
ANSI C37.13
ANSI C37.16
ANSI C37.17
ANSI C37.50
UL1066 (UL Listed)
NEMA SG3

Insulated Case Circuit breaker (drawout and fixted)
UL489 (UL listed)
NEMA AB1
CSA C22.2 No. 5.1 (CSA Certified)


CTA-ID : 6189
Was this helpful?
What can we do to improve the information ?