Technical FAQs

Ask a Question

Do the masterpact NW and NT breakers meet IEC vibration requirement?

Yes. Masterpact breakers meet IEC 68-2-6 Standards for vibration:
2 to 13.2 Hz and amplitude .039 in. (1mm)
13.2 to 100 Hz constant acceleration .024 oz. (.7g.)

CTA-ID : 6174
Was this helpful?
What can we do to improve the information ?