Technical FAQs

Ask a Question

Can you use the LH4N softstart on the single phase motor, split capacitor motor?

The LH4N1 ( soft starter ) can be use with single phase capacitor start motors. With this product we have only the soft starter possibility , not soft stop .
The LH4N1 can run also the single phase motors with brushes .
The LH4N2 can not be use with a single phase network because it asks the three phases on its input .

CTA-ID : 7533
Was this helpful?
What can we do to improve the information ?