Technical FAQs

Ask a Question

What are the repair parts for a D222N Series E03 General Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40566-670-50
Load base assembly - 40560-026-50
Arc shield - 40530-018-01
Lug assembly - 40251-016-52
Solid neutral assembly - SN03
Base assembly mounting screw - 21427-171-61 (3) required for line base & (2) required for load base.
Arc shield mounting screw - 40205-071-01
Solid neutral assembly mounting screw - 40205-065-01
Neutral bonding screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)


CTA-ID : 8284
Was this helpful?
What can we do to improve the information ?