Technical FAQs

Ask a Question

Do you get the lockable handle on all of the 8636, 8638 and 8639 enclosed Altistart ATS46 units?

Issue: Do you get the lockable handle on all of the 8636, 8638 and 8639 enclosed Altistart ATS46 units?
 
Product Line: Enclosed ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: Do not get this on the 8636 since there is no disconnect in the starter but is on the other enclosure types.


 
Was this helpful?
What can we do to improve the information ?