Technical FAQs

Ask a Question

Need to know what measurement he should get on the SCR`s of the Altistart ATS23 when check them from line to load?

Issue:   Need to know what measurement he should get on the SCR`s of the Altistart ATS23 when check them from line to load?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Told him should get greater than 30K ohms (30,000 ohms).


 
Was this helpful?
What can we do to improve the information ?