Technical FAQs

Ask a Question

What is the mounting information for the GC DSP display used with the GC-200 ground fault relay?

Drill or punch a hole 2 to 4 inches in diameter, for communication cable.
Drill 4 mounting holes using template. Use a 3/16 in (5mm) drill bit.
Tighten all screws to 6-9 lb-in. (0.7-1.0 NM)
Refer to Bulletin No. 48049-220-01 for mounting template.


CTA-ID : 8016
Was this helpful?
What can we do to improve the information ?