Technical FAQs

Ask a Question

How can I test the LH4N106RTY in an unloaded condition with causing my motor overloads to trip immediately?

Turn initial torque to its highest setting and acceleration to its lowest setting. Due to the fact we gate one SCR in the LH4N1 we have an imbalance at start up that is magnified in an unloaded state. Making these adjustments will allow bench testing without tripping properly sized motor overloads.


CTA-ID : 8014
Was this helpful?
What can we do to improve the information ?