Technical FAQs

Ask a Question

Why doesn`t FDA14015A come up as a valid catalog number on quote-to-cash?

FJA14015A is not a valid catalog number because of the ``A`` phase option at the end of the catalog number. The phase options for the FD/FG/FJ breakers are number ``1`` for ``A`` phase, ``3`` for ``B`` phase, and ``5`` for ``C`` phase. Therefore, the correct catalog number with ``A`` phase option is FJA140151.


CTA-ID : 8010
Was this helpful?
What can we do to improve the information ?