Technical FAQs

Ask a Question

What is Demand Metering on the new Micrologic x.0A trip units?

Demand Metering: The demand is calculated over a fixed or sliding time window that can be programmed from five to 60 minutes.
Maximum demand values are systematically stored and time stamped.

CTA-ID : 7979
Was this helpful?
What can we do to improve the information ?