Technical FAQs

Ask a Question

What is the Maximum recommended motor cable length to be used on the VSD07 without requiring an output filter?

100 feet is the Maximum recommended motor cable length. This can be found on page 14 of Instruction Bulletin ( 30072-450-07 ).


CTA-ID : 7237
Was this helpful?
What can we do to improve the information ?