Technical FAQs

Ask a Question

Can you stil order Rectivar units?

1.- If trying to replace and existing unit in the field can order through Q2C.
2.- If looking for a new drive then can obtain units from Systems group at 919-855-1197 to quote new system.
3. - If need to repair or troubleshoot one then go through your point of purchase for assistance.





CTA-ID : 7221
Was this helpful?
What can we do to improve the information ?