Technical FAQs

Ask a Question

Would it be ok to put a ground fault interuption (GFI) breaker between the Altivar ATV66 drive and motor which is a solid state device?

You should not use solid state devices between the drive and motor, it will cause ringing on the line and in turn cause nuisance tripping.


CTA-ID : 7199
Was this helpful?
What can we do to improve the information ?