Technical FAQs

Ask a Question

Is the identification for the Altivar ATV66 unit found on the power board or control basket?

The power board carries the drive identification so it will recognize what size it is and that is why depending on the range of units you can use only 2 control kits throughout.


CTA-ID : 7168
Was this helpful?
What can we do to improve the information ?