Technical FAQs

Ask a Question

Have Masterpact NW breakers met IEC standards for vibration?

MASTERPACT circuit breakers meet IEC 68-2-6 Standards for vibration.
2 to 13.2 Hz and amplitude 0.039 in. (1 mm)
13.2 to 100 Hz constant acceleration 0.024 oz. (0.7 g.)


CTA-ID : 7964
Was this helpful?
What can we do to improve the information ?