Technical FAQs

Ask a Question

What are the repair parts for an MPR33125, Series M01 Meter Pak Device?

Issue:
Current design repair parts

Product Line:
Meter Pak Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Customer Cover (includes labels) - MP3125C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Blank Meter Socket Cover (top position) - MMCBK
Meter Socket Cover (ringless type, one position) - MMRC
Pull Box Cover - MP34125PC
Line Phase and Neutral Lugs - MMLK250
Alternate Lug Kits - Refer to Digest
Load Neutral and Service Ground Lugs Assembly - 7329819855 (includes 5 lugs and bus bar the lugs are mounted on)
Mounting Screws for Load Neutral and Service Ground Assembly:
(1) 2142720163 - Mounts the top of the assembly to the Main Neutral Bar
(1) 2149020120 -  Mounts the assembly to the enclosure, just below the Main Neutral connection
(1) 2153217161 - Mounts the assembly at the bottom to the bracket attached to the enclosure

Equipment Ground Lugs Assembly - 7329897052 (includes 3 lugs and mounting bracket)
Mounting Screws for Equipment Ground Lug assembly - 2142217101 ( 2 required)
Parts Kit (one position, meter socket line side through tenant breaker base) - MM125KIT
Mounting Channel - 7329652001


CTA-ID : 6000
Was this helpful?
What can we do to improve the information ?