Technical FAQs

Ask a Question

Why does encoder not operate properly when the Altivar ATV66 drive is running and has added a line reactor, RFI filter, new ground, sheilded motor cable grounded at one end, and it still has not resolved the problem.

Try putting a Capacitor across the power terminals of the encoder. This may help filter out noise. May need to get a scope and work your way back to isolate where the problem is comming from. This is a wiring issue.

CTA-ID : 7026
Was this helpful?
What can we do to improve the information ?