Technical FAQs

Ask a Question

Would a standard Current transformer work on the output of the Altivar ATV66 drive?

Unless the CT is rated from 0-60Hz it will not read properly. You will want to contact the CT manufacture for more information.


CTA-ID : 7015
Was this helpful?
What can we do to improve the information ?