Technical FAQs

Ask a Question

What are the repair parts for a LA400R, Series E02 circuit breaker enclosure?<br />

Issue:
Repair Parts

Product Line:
Circuit Breaker Enclosure

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - LA400RC
Cover Mounting Screw - (2) 2142717161
Interior Trim - 4051549601
Interior Trim Mounting Screw - 4020513001K
Mounting Pan - 4051532701
Mounting Pan Hardware - (4) 2300100200 and (4) 4021200401
Handle Lock-Off - HPAFK (for K frame breaker), HPALM (for L frame breaker)
NOTE: Interior Trims do not have labels applied.


CTA-ID : 5975
Was this helpful?
What can we do to improve the information ?