Technical FAQs

Ask a Question

What are the repair parts for an EZM11200FSU, Series M01 main fusible switch unit?

Only the parts listed below are considered field replaceable:

Customer Cover (top compartment) - EZM11200FSUTC
Utility Cover (bottom pull box compartment) - EZM11200FSUBC
Cover Screws - 4020513002K
Molded Case Switch - PHF260000M
Fuses Required (order separately) Class T (300 Vac) 1200A max.
Keps Nuts (1/2``-13 nut) - 2342702800
Bonding Strap - 7329696754
Mounting Channel - 7329654305
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP

CTA-ID : 5949
Was this helpful?
What can we do to improve the information ?