Technical FAQs

Ask a Question

What are the repair parts for a QO330M125RB, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - 4056305550
Interior Trim - 4056305401
Interior Assembly - QO330M125RBI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - KDL32125
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142717161
Main Lug Mounting Keps Nut - 2342702000
Main Breaker Connecting Strap - 4055901901


CTA-ID : 7892
Was this helpful?
What can we do to improve the information ?