Technical FAQs

Ask a Question

Is the wiring the same on the ATV56 as a ATV66?

Yes to a large degree. The logic inputs and analog inputs are the same but may have different outputs depending upon option cards used on the ATV66.

CTA-ID : 6775
Was this helpful?
What can we do to improve the information ?